FemCap birth control
FemCap Non-hormonal birth control FemCap History About FemCap Non-hormonal birth control FemCap Clinician Protocol FemCap Non-hormonal birth control Directions How to order the FemCap
Advantages of FemCap Birth Control Female Birth Control FemCap Videos Female Contraceptive Links FemCap Female Contraception News FemCap Female Contraception Frequently Asked Questions Contact FemCap for superior non-hormonal birth control

Women Who Would be Very Successful Using the FemCap

  • Are highly motivated and educated
  • Can not tolerate the side effects of hormones
  • Have contraindications to IUDs
  • Who are allergic to latex rubber or do not rely on the
    male to use the condom

Women Who Would Tend to Have a Higher Failure Rate with The FemCap

  • Women who have used the earlier version of the FemCap (currently obsolete and not approved by the FDA)
  • Women who have aversions to touching their genitalia
  • Women who lack motivation and/or planning

Clinicians should help women choose the most suitable method for their age and lifestyle.

Ortho Women's Health a unit of Ortho-McNeil Pharmaceutical, Inc. inadvertently copied the information from the Prentif-cavity-rim cervical package insert yet displayed the FemCap photo in the above poster. Please see the correction below.

 


If a woman chooses the FemCap, the clinician should discuss the advantages, disadvantages, and the importance of compliance.


The Clinician should:






A)
Undersök livmodertappen för att utesluta eventuella missbildningar och bedöma storleken.


B)
Välj storlek på FemCap utifrån din obstretiska historia och undersökning av livmoder-tappen

Petite 22mm= Aldrig varit gravid
Small 26mm= Efter kejsarsnitt eller missfall
Regular 30mm= Efter vaginal förlossning

 

 

 

 

Studera DVDn och känn på livmodertappen,
öva därefter själv på att sätta in och ta ut FemCap


 

 

C) Är du osäker – låt en läkare eller barnmorska kontrollera att den sitter korrekt över livmoder-tappen.

FemCap training is relatively simple. Women may be able to insert and remove the FemCap in the squatting position ON THEIR OWN very easily and quickly.

The FemCap is held in place by the muscular walls of the vagina and does not have to be snug around the cervix or hinge behind the pubic bone. The FemCap has a brim that flares outward like an inverted funnel to direct sperm towards the groove that traps the sperm and exposes it to the stored spermicide; this is a difference between the FemCap and the diaphragm.

Copyright © 2007 - FemCap All Rights Reserved